9/20/2021 9:23 AM | |
Posts: 7 Rating: (0) |
Hi, everyone! I'm here to request assistance, please. I've been having problems simulating an HMI screen. I've set the corresponding tags for the PLC and HMI linked to the PLC's, and set the HMI connection between them. The HMI has several screens to check if the simulation is properly working, and I think it is because it actually changes screens, and even shows the animation (red for low level or zero) of the indicator. But I press the HMI button and it pops the "tag could not be written" alert, so it doesn't change to green (high level or one). I mean, I know it's weird that at first it says that is has disconnected, but the fact that lamp is red it means is reading something, or am I wrong? I even set the PG/PC configuration to S7ONLINE(STEP 7) --> PLCSIM S71200/S7-1500.TCP.IP.1 in control panel. I'll leave a link to drive so you can download the project to take a better look. [snip] I'll attach the image of the first error. Thank you for your attention. AttachmentFiles.zip (328 Downloads) |
Last edited by: Jen_Moderator at: 09/20/2021 13:24:16Removed link and added files as an attachment. |
|
9/20/2021 9:27 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
set the pg to PLCSIM.tcpip |
9/20/2021 9:40 AM | |
Posts: 7 Rating: (0) |
It didn't work |
9/20/2021 9:41 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
which SW Versions you use exactly? is PLCSIM running and the project is loaded? |
9/20/2021 10:03 AM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Hello, Have you seen this faq: Best regards, Wizard |
Follow us on