1/18/2019 12:47 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Hi, as from TIA V15.1 it is possible to build F communications over a "standard" communication. This is called as Flexible F-link . The SIOS docummentation shows an example here https://support.industry.siemens.com/cs/ww/en/view/54110126/116268117259. TIP: it is necessary to "acknowledge" the communication on the receive side. Attached I place a project example with this "tip". Differently of the official example, for simplify the cose, I used configured communication instead of the programmed communication. But configured communication is not a "must". AttachmentF.zip (326 Downloads) |
Last edited by: Jen_Moderator at: 1/21/2019 9:47:46 AMRemoved name. Denilson Pegaia |
|
This contribution was helpful to12 thankful Users |
10/3/2019 12:47 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Hi, here there is a second example, with bidirectional communication. AttachmentF_20190918_1000.zip (247 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to4 thankful Users |
Follow us on