12/26/2013 8:19 AM | |
Joined: 8/10/2009 Last visit: 7/19/2024 Posts: 166 Rating: (2) |
Dear Ashish , Its a Fixed Value Thanks Sarabjot Singh Manku
|
12/29/2013 1:37 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello What type of calculation are you performing ?In Practice Rounding the value to5 digits instead of8 digits ( Total 7 digits instead of 10 digits )would result in an inacurracy of < 10-7% which should be too small and can be ignored for most industrial applications. ( Unless of course you are calculating a trajectoryof a spacecraft to Mars ) Still if you feel that you really need this accuracy, you can use 64bit floating point numbers, although these are not easy to use in calculations inside S7 PLCs ) You can check outdchartier's comments in my previous post inUsing Double FLoat in S7 Cheers Navnag |
Last edited by: Navnag at: 12/29/2013 1:48 PMLast edited by: Navnag at: 12/29/2013 1:43 PMThere is no such thing as the last bug in a program |
|
Follow us on