10/12/2021 6:24 PM | |
Joined: 11/19/2018 Last visit: 3/27/2024 Posts: 7 Rating: (0) |
Hello Gentlemen, I am simulating a project using PLCSIM Advanced V3.0 (CPU 1517-3) and working in TIA V16. And this works fine. I added a touch panel (KTP900 Basic PN) in this TIA project, but I cannot simulate it. When I start simulation on the touch panel, somehow there is no connection to the "Soft PLC". I already set up the connection with using access point S7ONLINE. My question is: 1. Is this kind of configuration possible to be simulated ? (No real PLC and no real touch panel) 2. If this is possible, is there any step by step guide that I can follow ? And then can we simulate also touch panel with profibus protocol ? Or is it only possible touch panel with profinet protocol ? For more information: The PLCSIM Advanced and the TIA portal are on different PC environment. I can ping the "Soft PLC" IP address from my TIA working station. Thank you in advance AttachmentSimulation.zip (154 Downloads) |
10/13/2021 8:22 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8640 Rating: (1151) |
Hello, Perhaps this link might help: Best regards, Wizard |
10/13/2021 3:00 PM | |
Joined: 11/19/2018 Last visit: 3/27/2024 Posts: 7 Rating: (0) |
Hi, I found also this document and tried it. But it doesn't really help. Anyway, thank you for your information. |
Follow us on