5/19/2011 4:40 PM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, this FAQ may help you: How do you do an operating system update (OS update) on operator panels? But you don`t post a screenshot of your problem at the OS-update sadly. Wich error do you get there? best regards. |
5/29/2011 5:02 PM | |
Posts: 8946 Rating: (999) |
Because you are working with SP1, you have to do a downgrade of panel, using ProSave Software. |
5/29/2011 5:10 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
So, you will need a What connections are there between the version designations in WinCC flexible?...and of course3 Sandman link mentioned above. Best regards, Hristo Mihalev |
5/29/2011 5:16 PM | |
Posts: 8946 Rating: (999) |
No, that is not necessary. If WinCCflex2008SP1 is installed with the associated ProSave, The actual FW that you find on your harddisk is allready the FW that is good for your panel. Just doengrade and everything is fine. I do it a lot of times with different Panels, each time successfull. |
5/29/2011 5:20 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
The idea is was that member to understand where is the problem and then to follow Sandman link.... |
Follow us on