Industry Online Support
Technical Forum
2/17/2009 10:04 AM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151) |
Dear petermat, Have you seen this link: http://support.automation.siemens.com/WW/view/en/23802404 Perhaps it's useful. Best regards, Wizard |
2/17/2009 1:43 PM | |
Joined: 4/24/2006 Last visit: 5/13/2024 Posts: 8641 Rating: (1151) |
Yes, that's right.
No, you can connect notebook directly to hmi.
Yes, here is a link, how to transfer project using ethernet: http://support.automation.siemens.com/WW/view/en/23800567
When you transfer, there are some files transfered from PC to HMI. I do not know what happens when you transfered
HMI might be downloaded seperately, using ethernet. Best regards, Wizard |
This contribution was helpful to1 thankful Users |
2/17/2009 2:33 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello, You can transfer WinCC flex. project into the Windows CE based panels like MP277 using one of the following methods. 1. Ethernet; follow instructions in the following link: http://support.automation.siemens.com/WW/view/en/23800568 2. MPI/Profibus; follow instructions in the following link: http://support.automation.siemens.com/WW/view/en/23802404 3. USB; Please download the manual in the following link: http://support.automation.siemens.com/WW/view/en/22809353 With best regards. |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
Follow us on