5/8/2020 8:58 AM | |
Posts: 3 Rating: (0) |
Hi we have had a request from a customer about transferring a programme on a LOGO 6ED1 052-1HB00-0BA6 to a 6ED1052-1HB08-0BA0. The software we are using is LOGO V8 Demo version. I have managed to get the programme from 0BA6 by comparing it and copy and pasting onto a black sheet, then I have tried copying the 4 firmware files and programme onto a Micro SD card and putting it into the 0BA0 while it is powered down, so far I have been unsuccessful. Any help or step by step guide you could give me would be most appreciated, is it possible to do this with a demo version of the software and do both part numbers need to match for this to be compatible? I have also included a copy of the original programme. Kind regards Chris ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/08/2020 10:11:47New subject after splitting |
|
5/11/2020 1:25 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Import of a technical question of the User ChrisAth via PM:
The Update Center from LSC is unfortunately not working. You can download the update to the current version of Windows here: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) It is a 1.3 GB complete package.
|
This contribution was helpful to1 thankful Users |
Follow us on