11/4/2022 10:19 AM | |
Joined: 10/16/2022 Last visit: 11/4/2022 Posts: 3 Rating: (0) |
Hi, I already posted this question, but once again I'm trying to ask the same question. we have a concentration analyzer that stores the results of the analytics in the inbuilt operating system which runs on windows 10. So, once the measurements are done it will store the results as a text file. This analyzer with an inbuilt OS has only an ethernet and USB interface. Based on these results of the concentration, I need to build a control system that controls the dosing pump. Now I need to transfer these results in a text file as input from the analyzer to Simatic PCS 7 with CPU 410E which is installed on another computer and has to read the data on the particular line of the text file as an input. I'm merely not sure whether it is possible or not, but to implement this analyzer in the control system this has to be done. PS: I'm hereby attaching the photos of the analyzer along with the text file of the results. I'm literally new to this platform and have no programming knowledge any useful inputs will be really helpful. TYIA Attachmentexperiment-2021-11-10_14-59-30-result.txt (254 Downloads) |
11/4/2022 12:35 PM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7966 Rating: (162) |
Closed cause question posted twice. The second thread with the subject Tranfering Input from PC to PLC is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on