6/26/2014 4:53 PM | |
Posts: 24 Rating: (0) |
so i got a FB ( on sheet version program) and i've tried to find the meaning of some parametres. UEBW STBE STME |
6/27/2014 9:34 AM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Difficult to say Martin212 without seeing the whole block or at least the block header. It seems to be a in German written block that's what I would say. Maybe you can post us more of the block. Best Regards. |
Give us your feedback and show us your respect! |
|
6/27/2014 8:30 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Ok Martin212 , let me give it a try with my broken German
The block name "stoerung" means "failure" or "error" but that's the easy part. UEBW seems to be from "Ueberwachung" and should be "monitoring". That could be the error cause or an enable/disable function because there is an "OFF" connected to it. STBE is difficult to say, could be anything. While it is S36 I guess it's a reset push button but it could be the error cause as well if the block is used several times with different inputs. ZEIT is a time or timer I think you figgured that out already. STME I believe stands for "stoermeldung" or "stoerungsmeldung" and means "Error/Alarm-Indication" If you would have a printout of the block that would help us more for sure. Best Regards. |
Give us your feedback and show us your respect! |
|
7/1/2014 8:18 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, DW14 is not 0.4 seconds or 1,4 seconds. It loads the value from DW14 of the opened DB. Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
7/1/2014 8:25 PM | |
Posts: 24 Rating: (0) |
okay but what is the time preset of this timer ? |
7/1/2014 8:30 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello,
DW14 can be a value from HMI, a fix value in the DB or written from a block. You must look in the reference data and HMI. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
Follow us on