12/5/2019 8:03 AM | |
Posts: 1 Rating: (0) |
Hello, I have the same problem with PCS7 v 8.2. I have 3 Single Station. One of them is also ES and on this station login window shows only once after runtime is starting. Also in runtime "trend online" window and "Picture selection via measurement point" also don't show up. I see them when press Alt+tab but windows fot this aplications are invisible. Where there may be a problem, please help? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/05/2019 13:32:42New subject after splitting |
|
Follow us on