Industry Online Support
Technical Forum
4/9/2009 6:30 PM | |
Posts: 7 Rating:
|
I am using a laptop with dolphin plus to connect to the multiranger. I do seem to get echo profiles based on the level; as the level is closer to the xps 10 I recieve the profiles, once it has dropped I can't get them. The next time the tank is at a higher level I will set up Dolphin Plus to do a timed measure so that hopefully I can get an idea at what level we can no longer make profiles. I have made a few profiles as well as copied the parameters and attached them. Files ending in "circ" the info was gatherd while the tank was circulating (drawing product from the bottom of the tank and pumping into the top). Files ending in 'nociric" the tank was not being circulated but product was being added to the tank. Files ending in "unload" the tank is being emptied. Is there any info you can direct me to about how to interpret echo profiles? The tranducer is about 4' from where product is filled when circulating (I have been told that tranducers should be 14" from any object for every 10' depth. the tanks is 15' so That should be ample clearance shouldn't it?) Thanks for your time. Tim Attachmentalum3.zip (128 Downloads) |
Follow us on