12/28/2021 10:40 AM | |
Joined: 12/14/2013 Last visit: 8/30/2024 Posts: 19 Rating: (0) |
Hello. I try to connect IOT2050 Advanced to internet by USB but nothing happens. I try to change model but with 3 different phones (2 Samsung and 1 Sony) the effect is the same. Note that : - with old Samsung I connect IOT2040 without problems - I try to disable firewall on IOT - I try to enable connection plugging USB after boot and leave USB connected during boot There is some test I can do to fix this problem? Is it possible to set this connection manually? BR ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/28/2021 10:55:22New subject after splitting |
|
1/26/2022 2:43 PM | |
Joined: 12/14/2013 Last visit: 8/30/2024 Posts: 19 Rating: (0) |
Hello. The actual version uses base image V1.1.1 and was updated for node-red installation with iot2050-IPC-2.1_S0061 service-stick. The attached file is the bootlog from UART BR AttachmentBOOT 2050.txt (322 Downloads) |
Follow us on