5/23/2016 6:34 PM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Hi. I have a induction motor with 0,18kW/380V/60Hz and a Sinamics G120 CU 240-2DP of 11kW. The drive is parameterized in U/f control mode (p1300 = 0) and sometimes we need work with 6Hz (10%) but looks that the drive does not have enough torque with this low speed. My doubt if I can change the control mode from U/f to SLVC (p1300 = 20) even with this big difference of power btw Motor and Drive? If not, could you suggest parameters to change in U/f to improve the motor performace in low speed. Best regards. AttachmentSinamics_G120_CU240E-2DP.pdf (172 Downloads) |
Last edited by: Berg at: 5/23/2016 6:35:50 PMfile attached "Educate the children and it won't be necessary to punish the men." |
|
5/23/2016 9:03 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (152) |
You must be joking. |
Follow us on