12/21/2017 3:49 PM | |
Posts: 2 Rating: (0) |
All, I would appreciate any help in trying to upload a program from an S7-1200 PLC. It appears that I have successfully made a connection and that I am online (Orange Title Bar), but I am not getting an option to upload (The upload button is grayed out). I have an "incompatible" error but what is incompatible, I don't know. I have attached a PDF with some comments and a screenshot. Thanks Colm. AttachmentS7-1200 - No Upload Option.pdf (408 Downloads) |
12/27/2017 11:43 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2372)
|
In that case, it could also be V13 SP1, V13, V12 (doubt it and aggg hope not), V11 SP2 (doubtful) If you use the online access in the project tree, you can look at the plc diagnostic buffer, diag status, plc part #, firmware revision, serial # and a few other things. Take a look at it. There is a tool you can download from the Siemens web site that allows you to upload and download projects to / from a PLC. SIMATIC Automation ToolYou can also insert a properly configured and acceptable S7-1200 compatible memory card to pull the project off the plc. Then you can look at the file extension of the project on that card (by opening that memory card on your PC) to see what major version is used. I do not recommend this option, but it will work.
|
science guy |
|
7/8/2020 8:19 AM | |
Joined: 3/14/2019 Last visit: 6/5/2023 Posts: 6 Rating: (0) |
if the CPU supports the web interface, then it will indicate the TIA version |
Follow us on