5/13/2021 2:05 PM | |
Posts: 198 Rating:
|
Hello Nikola, Usually in the upgradation perspective, there are two options: with or without the utlilization of the functionality of the newer version (9.1 in this case). It is recommended to go through this manual perform the upgradation based on your requirement: SIMATIC Process control system PCS 7 Software update with utilization of new functions V9.1 SIMATIC Process control system PCS 7 Software update without utilization of new functions for SIMATIC PCS 7 V9.1 On that note, Siemens only provides recommendations and procedures with relevance to the PCS7 product line. PCS 7 can only run on operating systems that have been approved for PCS 7 (but Siemens does not recommend whether or not you could upgrade the OS or not - Before installing PCS7 v9.1, it is important to ensure one of the recommended OS is installed). Also with 9.1, the SQL version is different (SQL 2017) and hence, there could be possibilities of issues coming up with your proposed possibilities of OS upgrades which are not clear as yet. It is recommended by PCS7 to follow the guidelines for recommended Operating systems and IPC product line for a trouble free upgrade experience. Hope this helps. |
This contribution was helpful to
1 thankful Users |
12/14/2021 12:11 PM | |
Posts: 2 Rating:
|
Please, Share with me your experience as I am facing similar kind of situation. Thanks, Awais Sattar, |
Follow us on