2/21/2015 10:37 AM | |
Posts: 1 Rating:
|
Hi All, Being a newbie with Logo, I guess I have a newbie question here, nevertheless, hope someone can help. I have a simple scenario (to become part of a larger program) in which I want to set the offset time of an off delay via the cursorkeys of an TDE module. So far I can use the up and down arrows to increment a Up/Down Counter. What I don't manage to do is using that value as a reference in my off-day. I've seen other samples where the offdelay was controlled by a reference. But when I look at the block properties of my off-delay, I don't see an option to use a reference. How can I link/use the counter of my Up/Down Counter as the input for the Off-day? Attached the schema. Thanks in advance! AttachmentControlKeyTest.zip (242 Downloads) |
This contribution was helpful to
1 thankful Users |
2/21/2015 10:58 AM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33445 Rating:
|
Look at this link: https://support.industry.siemens.com/cs/#document/109471094?pnid=13617&lc=en-DE |
This contribution was helpful to
1 thankful Users |
Follow us on