5/12/2012 8:39 AM | |
Posts: 58 Rating: (19) |
Dear Ani, I have attached the Starter backup of one of our projects. The application there was for controlling feed roll in a "Cut to Length Line" for cold rolled coils. The drive name is Feed_Roll_Drv where we have used basic positioner and position control. Here we have used 37kW S120 PM for driving a 34kW asynchronous motor having a 1024 ppr incremental encoder. The project was created using Starter version V4.2. You can learn the concepts for basic positioner and position control from the function manual (Chapter Function modules). Please download the latest function manual at the following link: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=13305690&treeLang=en Regards Ajay Gupta AttachmentCTL_1_All_Drive_As_Commissioned_Bkup.zip (1034 Downloads) |
This contribution was helpful to1 thankful Users |
5/14/2012 11:40 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi you can use this sample also with regards ram AttachmentEta_p130.zip (886 Downloads) |
This contribution was helpful to1 thankful Users |
4/29/2015 11:20 PM | |
Joined: 9/9/2012 Last visit: 7/8/2024 Posts: 11 Rating: (1) |
Dear Ajay can you send me the complete program of the ctl-1 including plc. Regards Deepak kumar |
Last edited by: Min_Moderator at: 4/30/2015 10:12:46 AMRemove contact data |
|
Follow us on