5/25/2011 1:41 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi I agree wizard, rs 232 if possible. /tf/WW/en/Posts/47986 If you mean pci, there is pcmcia like cp5612cards, but I think it´s not for Step 5/S5. I using PG and original cable 6ES5734-2BF00. If not laptop http://www.automation.siemens.com/mcms/industrial-communication/en/profibus/system-connections-pg-pc/cp5613a2/Pages/cp5613a2.aspx Regards Heksu |
Last edited by: Heksu at: 5/25/2011 8:41 PMLast edited by: Heksu at: 5/25/2011 1:43 PM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
5/28/2011 1:52 PM | |
Posts: 21 Rating: (3) |
There are also USB-Adapter-Cables available; but be carefull - that have to be specal adapters (not "normal" USB to RS232), this is a special hardware with a windows-driver specially for S5-Online for examle see here: S5-Online USB or goggle for it |
6/1/2011 8:40 PM | |
Joined: 6/13/2010 Last visit: 5/29/2024 Posts: 35 Rating: (0) |
try www.process-informatik.de works OK |
6/5/2011 11:17 AM | |
Posts: 259 Rating: (5) |
Hi, Maybe this will be interesting for you I attach photo of cable that I use to connect with PLC S5. With regards, makaveli AttachmentCable.part1.zip (299 Downloads) |
6/5/2011 11:19 AM | |
Posts: 259 Rating: (5) |
Second part of attachment. I compressed with rar. With regards, makaveli AttachmentCable.part2.zip (301 Downloads) |
Follow us on