9/14/2012 9:21 AM | |
Joined: 1/8/2007 Last visit: 1/5/2024 Posts: 21 Rating: (1) |
The MMC is to update the firmware version without Step7 Best regards...
|
9/14/2012 9:32 AM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Is it only for update? |
9/14/2012 9:32 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hello, Have a look at this link: New ET 200S Interface Modules with PROFINET IM151-3PN Standard and High Feature Interface Released for Delivery With these modules it is not necessary to use MMC for operation. The older interface modules needed an MMC to save the Device Name. Best regards, Wizard |
This contribution was helpful to2 thankful Users |
9/14/2012 11:39 AM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Thanks Wizard! Subject closed! Greets, Nick |
This contribution was helpful to1 thankful Users |
Follow us on