11/5/2019 1:52 PM | |
Joined: 11/7/2011 Last visit: 1/27/2023 Posts: 96 Rating: (0) |
DEAR SIR, I AM USING PROFIBUS ABSOLUTE ENCODER OF LEINE & LINDE WITH S7-400H SYSTEM(SIMATIC MANAGER),I HAVE NEVER USED PROFIBUS ENCODER ,HOW TO READ THE ENCODER BY CONFIGURING AS Class2 32 bit Velocity AS DP V0).I HAVE ATTACHED GSD FILE MY DOUBTS ARE FOLLOWING:- 1. HOW DO I RESET THE ENCODER(WHICH BIT/WORD IS TO BE FORCED ) 2.FAULT BIT OF ENCODER 3.READ THE ENCODER VALUE(MULTITURN) 4.READING THE INSTANT VELOCITY. THANKS & REGARDS, SAMIR ------------------------------------------------------------------------------------------ AttachmentEncoder_PROFIBUS_DPV0_and_DPV2.zip (202 Downloads) |
Last edited by: Jen_Moderator at: 11/05/2019 14:19:37New subject after splitting |
|
11/5/2019 3:09 PM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4148 Rating: (464) |
The questions you have, should be found from the encoder manual. |
Follow us on