5/30/2008 4:14 PM | |
Posts: 510 Rating: (117) |
Wave, The Berger book, Automating with Step 7 in STL and SCL is an excellent reference for SCL programming. It includes programming examples. I have attached the SCL examples. Blocks created in SCL are entered in the Blocks folder after a successful compile. The FC and FB blocks can be called in the LAD or FBD editor just like blocks created in STL/LAD/FBD. There are system attributes required if the SCL generated blocks are going to be used with CFC, PDIAG, Graph, and HiGraph, but there are none that are required for LAD/FBD. Bill AttachmentScl_book.zip (906 Downloads) |
9/23/2008 3:00 AM | |
Posts: 2 Rating: (0) |
Thanks for uploading that same SCL File. Do you have an EBook of Automating with Step 7 in STL and SCL? |
9/23/2008 3:57 PM | |
Posts: 487 Rating: (44) |
I do not think the book is available in E-format. |
9/23/2008 7:48 PM | |
Posts: 2 Rating: (0) |
Thank You JMJ |
Follow us on