Industry Online Support
Technical Forum
2/6/2014 6:53 AM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
the dip switch on the new E / R modules have been set?
|
2/6/2014 10:20 AM | |
Posts: 118 Rating: (1) |
Hi, yes S1 switch settings were 1 and 6 are on, ensured this is the same on the new module |
2/6/2014 12:50 PM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
check powermodule Z Axis if it possible change Z Axis PM with X or Yaxis |
2/6/2014 1:11 PM | |
Posts: 118 Rating: (1) |
I was going to try this but the x axis is 50amp power module on its own, the b/c axis are 2x15amp power modules and y/z is 2x25amp. |
2/25/2014 9:00 AM | |
Posts: 118 Rating: (1) |
Hi the issue is resolved, the e/r module i replaced was also faulty!. Fitted new one and all ok. |
Follow us on