1/7/2020 9:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi, what about installing this HSP? Support Packages for the hardware catalog in the TIA Portal (HSP) |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
1/7/2020 9:55 AM | |
Joined: 9/10/2013 Last visit: 11/27/2023 Posts: 3 Rating: (0) |
yes I have installed. But v2.0 and 3.0 do not
|
Last edited by: auto_1971 at: 01/07/2020 09:59:17 |
|
1/7/2020 10:17 AM | |
Joined: 9/10/2013 Last visit: 11/27/2023 Posts: 3 Rating: (0) |
the problem is not over |
1/7/2020 10:47 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi, I´ve looked into the contents of the HSPs for V16.There is no HSP0185 V2.0 or V3.0, only V1.0 exists. If I where you, I would ask Siemens directly to this behaviour. Start a Support-request hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
1/8/2020 2:22 AM | |
Joined: 10/7/2009 Last visit: 9/9/2024 Posts: 266 Rating: (92) |
Hi, Just wondering, have you really installed the "HSP0185 - SINAMICS V90 PN – FW-Version 1.04" downloaded from the link mopS04 provided? "TIA_Portal_V16_HSP.zip" If this HSP is already installed, you should see "HSP0185 SINAMICS V90 PN V4.0 in TIA V16 > installed" (picture attached) and the upgrade of your project from V15 to V16 will be successful (just as I did).
Best regards, Yu-Wen |
Follow us on