12/6/2018 9:34 AM | |
Posts: 5 Rating:
|
Dear experts, I am trying to control SINAMICS V90 PN servo system (see attachment) with S7-1214 DC/DC/DC. I have gone through a few application examples where they recommend to use standard telegram 3 (see attachment) for position control with S7-1200. However, I don't find telegram 3 among the available list in V-Assistant (see attachment). I am using TIA V13 SP1. So far, the motor shaft rotates when JOG from V-assistant but when trying to JOG from the TO it does not rotate (I think because telegram 3 is not selected) Would highly appreciate your quick responses AttachmentV90_attachment.pdf (297 Downloads) |
Last edited by: Mahmoud Sakr at: 12/6/2018 9:35:26 AMLast edited by: Mahmoud Sakr at: 12/6/2018 9:38:21 AM |
|
12/6/2018 10:31 AM | |
Joined: 5/12/2006 Last visit: 7/8/2024 Posts: 22299 Rating:
|
Hello, here the application example: https://support.industry.siemens.com/cs/ww/en/view/109743917 Regards Christoph |
12/6/2018 12:35 PM | |
Posts: 5 Rating:
|
Hello, I did a factory setting reset to the drive and configured it again and it seems to work. Many thanks Christoph Regards, Mahmoud |
Follow us on