5/6/2022 2:34 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello Tatzmon, I still don't really understand the problem. The order is incorrect if the count or the components to be entered have two digits? Perhaps the FAQ will help you. It is also entered here from top to bottom, but one byte is reserved for each character so that there is no confusion during the order. How do you convert a character string into single character bytes in STEP 7 V5.5? With best regards |
5/26/2022 10:29 AM | |
Joined: 4/23/2010 Last visit: 1/11/2023 Posts: 5 Rating: (0) |
Hi Cicero, I use blockmove with specific byte length. I want to re-arrange the characters from top to bottom into bottom to top. Is there a way of doing it shortly? Regards, Tatzmon |
Follow us on