7/8/2024 9:51 AM | |
Joined: 5/30/2022 Last visit: 7/30/2024 Posts: 556 Rating:
|
Hi hjamshidi, Why don't you communicate with the other PLC via one of the communication channels available via WinCC? If it is not a Siemens PLC you have the option of communication for example by OPC UA or by OPC DA. In this manual: WinCC V8.0: Configuration and communication all the possibilities come. By script, you would have to see some example of Open TCP/IP communication by visual basic although the recommendation would be to do it directly by the channels that WinCC integrates. |
If this information really helps, you could use the Rate function. |
|
Follow us on