Industry Online Support
Technical Forum
2/24/2012 5:55 AM | |
Posts: 165 Rating: (25) |
Hello experts, We are facing one serious problem with the Basic Line Module of 100kW. BLM shows the fault "F30021 Power unit: Ground fault V4.4". We checked the wiring and all ... all are ok...No line to ground fault present inside the panel.. Finally we decided to use a new BLM instead of that faulty one. We give only 24 V dc power supply to the new BLM unit for testing purpose(after discussing with siemens technical person). This time the new BLM shows the following fault code: "F30025-Power unit: Chip overtemperature V4.4" "F30005-Power unit: Overload I2t V4.4" Why this is happening? The BLM is operated with SINAMICS S120 CU320 control unit, four servo drive and one Braking module. I have attached the screen shot of the faults (for new BLM).... This is the BLM detail: 6SL3130-1TE31-0AA0 100kW Please let us know as soon as possible... Thanks Regards Mothilal Attachmentblm_china_f30005_f30025.zip (200 Downloads) |
Last edited by: Mothilal at: 2/24/2012 5:56 AM |
|
Follow us on