Industry Online Support
Technical Forum
5/23/2010 12:17 PM | |
Posts: 62 Rating: (0) |
Hello to all, I have a WinCC flex Project that is running on a PC and would like to know if i can view this same project on a MP277 or do i have to create a new project again then download to HMI. Both the Pc and the HMI are connected to the PLC via ethernet. There is currently no project downloaded to the HMI. this is new. On the PC i am running WinCC flex 2008 SP2. I am not sure if i need to check the box Sm@rtACess or Service under Runtime service. Thank you expert for any help rendered. Regards, Raymond. |
5/23/2010 1:26 PM | |
Posts: 62 Rating: (0) |
Thaank you very much. I shall try this. Regards, Raymond., |
Follow us on