Industry Online Support
Technical Forum
11/29/2009 12:37 PM | |
Posts: 2 Rating: (0) |
I have WinCC V7.0 SP1 WinCC Web Navigator V7.0 Installed on RACK PC 847B with Windows 2003 Server (SP2) operating system. I also have Two numbers of Thin client. I am configuring the system with the help of " Distributed Operation of SIMATIC WinCC using SIMATIC Thin Clients" doccuments. Entry ID 28309119. While configuring I stuck on page no-49/73. After right clicking on Web Navigator option in Demo project WinCC explorer, I am not finding Web Configurator and Web Settings options. I skipped Web configurator and done with the remaining procedure. when i entered http://localhost/ in internet explorer its not working. Installed internet explorer is V6.0 SP2. Cananybody please extend some help in the issue? |
11/30/2009 8:55 AM | |
Posts: 45 Rating: (3) |
Hi! Have u installed the option web navigator? :) |
Follow us on