5/28/2019 9:10 AM | |
Posts: 5 Rating: (0) |
Hi, I have similar problem, but with array. I using TIA V13 SP1. I want to use array of char's, in FC I have an input block_db and I want to use this array as an input to another function. A used a temporary fix where I copied in cycle char by char to temporary array for next use. FOR #j := 0 TO 7 DO What is syntax for indirect addressing of an arrays? Thanks, regards, Viktor ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2019 13:52:22New subject after splitting |
|
5/28/2019 4:12 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello VkrSip, if you use the S7-1500/S7-1200 in TIA Portal there are two FAQs regarding to the indirect addressing methode: How in STEP 7 (TIA Portal) V11 do you program the data type "VARIANT" for indirect addressing for the S7-1200/S7-1500? How do you implement an array access with an S7-1200/S7-1500 with variable index? Cicero |
Follow us on