1/10/2023 10:27 AM | |
Joined: 11/28/2022 Last visit: 8/19/2024 Posts: 18 Rating: (3) |
When dynamizing an object property with a script, how does the trigger work when connected to a tag? Use case - defining the output format of an IO field in a faceplate with a script. I only need to run the script when the faceplate loads. I could declare the script in the "load" event of the faceplate, but would rather declare it within the dynamization of the object property. Edit - for this use case, the "load" event of the faceplate is the most suitable call environment for the script. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/10/2023 12:56:16New subject after splitting Last edited by: Zed1 at: 01/20/2023 11:16:21 |
|
Follow us on