8/2/2017 7:13 PM | |
Joined: 2/2/2017 Last visit: 4/27/2024 Posts: 36 Rating: (4) |
Hi, a question about eth1. When I connect the ethernet cable the orange led lights on, but the green one is off. Also It seems the port doen't acquire an ip address form DHCP. This is my /etc/network/interfaces: # /etc/network/interfaces -- configuration file for ifup(8), ifdown(8) # The loopback interface auto lo iface lo inet loopback # Wired interfaces auto eth0 iface eth0 inet static # address 192.168.200.1 address 192.168.10.29 netmask 255.255.255.0 auto eth1 iface eth1 inet dhcp It is the orginal one, with change to the static ip of eth 0. The led is off on my three IOT2040. It seems that the green led of X2P1LAN goes on only after a reset (by push button). Power off/on of the IOT leaves the led off. Obviously with a ethernet cable connected! Note that if all ethernet ports are disconnected from cables, after reset (by means of the reset button) the two green leds are on. X1P1LAN green led works always ok. Thanks for your help ------------------------------------------------------------------------------------------ |
Last edited by: cri2017 at: 8/2/2017 8:03:22 PMLast edited by: Jen_Moderator at: 8/3/2017 1:36:45 PMNew subject after splitting |
|
8/3/2017 8:57 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi, the LED does not behave as expected. The behavior is described here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on