Industry Online Support
Technical Forum
10/27/2009 7:49 AM | |
Posts: 15 Rating: (0) |
You didn't write what version(SP,hotfixies)of the WinCC server/Client are you using? |
10/27/2009 8:13 AM | |
Posts: 12 Rating: (1) |
I used WinCC V6.2 SP2 and I installed Windows server 2003 R2 on both HMIServers. |
10/27/2009 9:30 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Tanawat, could you tell more about your configuration? - are you using OS Client with project or without? - did you run Os project editor to create system page or not? - all station with same users and same password? (NO BLANK pawword) - all user in right windows user group? With more infor more expert can help Reagrds |
10/28/2009 3:22 AM | |
Posts: 12 Rating: (1) |
Hello, - are you using OS Client with project or without? => I used Client with project. - did you run Os project editor to create system page or not? => I didn't run OS project editor. - all station with same users and same password? (NO BLANK pawword) => HMIServer1 and HMIServer2 have the same but different with Clients and no blank password. And I used auto-logonaswell. - all user in right windows user group? =>All user are in thee same user group. Best regards, Tanawat AttachmentHMIServer.zip (28 Downloads) |
10/28/2009 7:37 AM | |
Posts: 15 Rating: (0) |
Hello Tanawat, do you use Pas CC V6.0x on the WinCC server/client stations ? Peter |
10/28/2009 8:45 AM | |
Posts: 12 Rating: (1) |
I used PASCC V6.0. |
Follow us on