3/20/2020 2:38 PM | |
Posts: 2 Rating: (0) |
dear. i have step 7 professional 2010 v5.5 and when istalling wincc FLEXIBLE 2008 but when setup is running all of sudden an error dialog box appearing with a masseage file not found F:\WINCC FLEXIBLE 2008 SP3\INSTDATA\SQL starter\SQLStarter.exe while i have installed microsoft SQL server 2005 express edition and 2008 is already installed ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2020 08:58:57New subject after splitting |
|
4/6/2020 4:27 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello Can you send us a Screenshot of the Error Situation? Which Simatic SW do you have installed? Do you use the Original DVD or have you downloaded the Installation Files from
Which Operating System do you use? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on