2/26/2019 4:18 PM | |
Posts: 1 Rating: (0) |
Hi, I used the TIA Porta V15 and make a Configuration with the CPU 1516-3 PN/DP. I have the following Problem : In our Profibus Slave was included in the GSD File the properties F_CRC_Seed and F_Passivation for a ProfiSafe Module F_Ext_User_Prm_Data_Ref(4) = 103 ;F_CRC_Seed F-Param-Flag1 (Motorola-Format einhalten!) F_Ext_User_Prm_Data_Ref(5) = 104 ;F_Passivation F-Param-Flag2 (Motorola-Format einhalten!) The GSD was compiled error free and installed successful in TIA Portal, BUT when I try to configure the Module in the Slot, (to move the Modul to the Modul zone), the modul was not inserted. (Observation during the move, the cursor show that it is possible). is it necessary to include Additional Configuration Parameter in the GSD file? what I missed? Thanks a lot for you help. Best Regards. Karen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/27/2019 10:52:33 AMNew subject after splitting |
|
2/27/2019 11:13 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi Karen, Which PB-slave do you use exactly? Did you choose a failsafe-CPU? regards, |
FCK WAR! |
|
Follow us on