1/25/2013 7:36 PM | |
Posts: 139 Rating: (0) |
hi guy which licence i need for my project: my project has 8000 tags and i need to archive all of them(in wincc 7.0 sp1) |
1/26/2013 2:44 PM | |
Posts: 36 Rating: (0) |
Hi In wincc 7 u must authorize by license keys and u need "Simatic_EKB_Install" with related keys. hope this was helpful
|
1/26/2013 4:01 PM | |||||
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683) |
Hello Avant; WinCC will come either as a complete (RC) package, allowing development anmd runtime, or as a RT (runtime) license only. On the RT systems you can oly operate and archive the project, you cannot do any development. Here is some information on WinCC licensing (look at the Product Information tab, for a description, and then search the Ordering Data tab to locate the exact license you need), along with some links https://eb.automation.siemens.com/mall/en/WW/Catalog/Products/10042373 Design SIMATIC WinCC is available as a complete package and as a runtime package with 128, 512, 2048, 8192, 65536, 102400, 153600, 262144 PowerTags 1). About archiving: - Integrated in the basic RC/RT licenses
- - Add-on tag licenses for archiving
Look also at the CAS (central archive server) option here: http://www.siemens.com/wincc/options For 8000 tags, you could start with an WinCC 7.0RC license for 8192 PowerTags (for the development computer), this weill allow development and runtime from this compouter, If you need to deploy other computers where no development is needed, then select the equivalent RT license. If later you find that you need more tags (with 8192 tags you are borderline) then you can selecta RC or RT PowerPack that will increase you PowerTag count. You wouyld also need an extra archive license; I showed the links for an RT archive 10000 point license, there are others in the Order Data tab for more part numbers. Hope this helps, Daniel Chartier |
||||
Last edited by: dchartier at: 1/26/2013 4:17 PM |
|||||
This contribution was helpful to3 thankful Users |
1/27/2013 1:24 PM | |
Posts: 139 Rating: (0) |
HI ALIFAEZ CAN YOU TELL ME WHICH LICENCE IS MY NEED EXACTLY? |
1/28/2013 2:07 PM | |
Joined: 2/22/2006 Last visit: 8/28/2024 Posts: 290 Rating: (37) |
Hi, You need: WINCC SYSTEMSOFTWARE V7.0 SP3, RC 8192 (8192 POWER TAGS), RUNTIME & CONFIGURATION, ON DVD, FLOATING LICENSE, 5 LANGUAGES (GER,EN,IT,FR,SP), EXEC. UNDER XPPROF/ WINDOWS7 (32/64 BIT)
This license will allows you to have up to 8192 external tag in your project and have up to 512 Tag Logging Archive tags. If you want ot optimize the price, you can use: WINCC SYSTEMSOFTWARE V7.0 SP3, RT 8192 (8192 POWER TAGS), RUNTIME, ON DVD, SINGLE LICENSE, 5 LANGUAGES (GER,EN,IT,FR,SP), EXEC. UNDER XPPROF/ WINDOWS7 (32/64 BIT) It has the same number of tags but it is not possible to using WinCC editors. To alifaez: Hi mate, using "Simatic_EKB_Install" is illigal - you know that. regards, Yolov |
6/5/2018 11:14 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by msn2212 is split to a separate thread with the subject At Run Time it show less Wincc Archive License tags than it should. Best regards |
Follow us on