11/9/2020 12:57 PM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Please also see the attached screenshots. I have just updated WinCC on my PG from 7.4 Upd. 1 to 7.5 SP1. I did not get any error messages and I can open both the Tag Manager, the Graphics Designer and the Cross-reference - but when I start an OS simulation I cannot operate anything - I cannot: Change the User Change the picture shown (I can see I an "pushing the buttons" but the picture does not change) What am I missing and how do I correct it? AttachmentWinCC Sim.zip (30 Downloads) |
Last edited by: xmnj at: 11/09/2020 12:58:43Added attachment |
|
11/9/2020 2:12 PM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hello Georg, Thank you for answering. Please see the attached screenshots. As far as I can see the "process script.exe" is not running. I have attached the "WinCC_Sys_0x.log" file since I cannot read it it and make any sense out of it .
AttachmentWinCC Sim A.zip (31 Downloads) |
11/9/2020 3:26 PM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hello again Georg, Please see the new screenshots. I will start the OS simulation again and look under details. Regarding the log file I hope it is a good sign that there is no entries since 19.08-2020? It is a WinCC 7.4 Upd. 1 I have updated to 7.5 SP1 (but I have not yet installed the 3 updates you recommended - do you think that is the solution to this problem too?). As far as I can see the "process script.exe" is also not listed under the "Details" tab. I did not install any of the 2 possible "Communication packages" - could that be the reason and which one should I install? I have to do something else tomorrow but I hope I can get back to this problem on Wednesday.
AttachmentWinCC Sim B.zip (23 Downloads) |
11/12/2020 10:23 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
After installing the 4 updates Georg recommended in another thread and which can be found here: https://support.industry.siemens.com/cs/de/en/view/109773812 the OS simulation can be used and I can log in as a different User and change the shown picture. |
Follow us on