5/9/2024 4:22 AM | |
Joined: 5/26/2016 Last visit: 5/9/2024 Posts: 8 Rating: (0) |
Does anyone have any idea why editting comments "//This is a comment" is so slow in the STL editor ? There should be no processing going on because the //i is already in the line and I'm editing on the right ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2024 03:54:17New subject after splitting |
|
5/10/2024 3:16 PM | |
Joined: 7/7/2010 Last visit: 10/7/2024 Posts: 15270 Rating: (2422)
|
Which portal version, which PLC family? If it is for s7-1200/1500, why use STL since that is an emulated system - especially if you have to comment the (presumably new) code. For s7-1x00, use SCL which runs as compiled directly into cpu code - instead of STL which runs inside an emulator within the PLC.
|
science guy |
|
Follow us on