10/14/2018 3:46 PM | |
Posts: 5 Rating: (0) |
Guys, I understand this is unrelated, but this is my first time here. could someone please answer my question or tell me where to posted? I am facing a commissioning deadline. I am using CONT_C in a function block. I call the FB in a Cyclic Program (OB32). when the PID is in manual I can change the Block CV by entering a manual value of 0-100%. The problem is starts when I put the loop in Automatic. It is a simple Flow control loop. As soon as I put the loop in Automatic, the loop becomes very unstable. Proportional gain is 0.1, Ti is 0 ms, PV_FAC=1. Derivative is also 0. SP=1100, PV (0-1800). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/15/2018 9:00:05 AMNew subject after splitting |
|
10/14/2018 3:52 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32989 Rating: (4076) |
Which software you use? |
10/15/2018 9:09 AM | |
Joined: 6/19/2017 Last visit: 5/8/2024 Posts: 8002 Rating: (163) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on