2/1/2017 8:33 AM | |
Joined: 10/11/2006 Last visit: 7/7/2022 Posts: 5231 Rating:
|
Dear s.kapil, this behavior seems to be caused by changing mechanical parameters: Maybe once you are moving a piece the control is stable. In a second try you might have a heavier piece moving and the parameters of controller settings are not valid anymore. You need to find a more robust setting. To do so you can follow the guidelines of: https://support.industry.siemens.com/cs/ww/en/view/60593549 In case you switch over from "with encoder" to control "without encoder" the controller settings should be adapted as well. If you don't achieve any improvement you should contact the SIEMENS Hotline by creating a request: https://support.industry.siemens.com/My/ww/de/requests#createRequest |
With best regards, |
|
Follow us on