Industry Online Support
Technical Forum
10/23/2009 9:48 AM | |
Posts: 18 Rating: (4) |
Dear members, I have a problem with freezing of client. (runtime freezes except event and alarm list - all indications are frozen, not possible to control) Configuration: Server: WINDOWS 2003 R2 SP2 + WINCC V6.2 SP2 HF5 + PASCC V6.01 TOPOLOGICAL HOTFIX CLIENT1: WINDOWS XP SP2+ WINCC V6.2 SP2 HF5 RC + PASCC V6.01 SP2 HF1 TOPO HOTFIX CLIENT2: WINDOWS XP SP2+ WINCC V6.2 SP2 HF5 RT + PASCC V6.01 SP2 HF1 TOPO HOTFIX After starting the project, one of the client always freezes (last is CLIENT2 22.10.2009 17:40) Second client (in this case CLIENT1) and the SERVER works OK. I am attaching diagnose files from all 3 computers. Best regards. Michal AttachmentDiagnose.zip (74 Downloads) |
Follow us on