1/20/2010 1:46 AM | |
Joined: 7/1/2008 Last visit: 10/13/2022 Posts: 15 Rating: (4) |
Dear SHAH@STERLITE Please check your user account is member of "SIMATIC HMI" & "SIMATIC HMI CS" after that make the following setting in the Simatic Menu Go to Simatic\SIMATIC Security Control\ Make Settings "C:\Program Files\SIEMENS\Common\SimaticSecurityControl\ssc_visual.exe" --repos="all" after that press apply & check it also Note last time i solved my issue by myself because of network sharing resource is bloked by windows and after release that one the wincc working normal. |
This contribution was helpful to2 thankful Users |
9/26/2011 1:03 PM | |
Joined: 11/17/2008 Last visit: 6/8/2023 Posts: 1 Rating: (0) |
Dear everybody, I have exactly the same problem than you, I try to open a multiclient project and I receive a a windows screen "The user does nothave the right to perform this action!" On the PMDIAGNOSE.LOG I receive: CCProjectMgr.exe Getsecurityinfo failed with error 5: Access is denied. The project could not be loaded from the server to the multiclient. In PMDIAGNOSE.LOG I receive: ccProjectMgr.exe CSingletonProject::AttachDatabases pICCDBManagement->AttachDatabase \\SIEMENS-CLIENT2\DATA\Project\MC_SERVERVIEW\MC_SERVERVIEW.mdf on SIEMENS-CLIENT2 failed: 0x80010105 It's a new installation of windows and winCC V7.0 SP2. |
5/4/2022 9:59 PM | |
Joined: 11/6/2021 Last visit: 1/16/2023 Posts: 15 Rating: (0) |
Hi sks_karthik. What network share did you exactly release and how did you do it?
|
Follow us on