9/18/2018 1:22 PM | |
Joined: 3/9/2012 Last visit: 5/22/2024 Posts: 236 Rating: (0) |
Hello, i want to use Web Server In Wincc 7.4 how can i do that? |
9/18/2018 2:36 PM | |
Joined: 8/5/2008 Last visit: 5/22/2024 Posts: 60 Rating: (10) |
Hello, It is very easy with Web Navigator. The short description is that you install the feature from the WinCC DVD. You make the needed configuration in your project(add graphics, publish the web site and pages via WinCC Explorer) and in WinCC User Administration. You can use the Web Viewer RT for testing in case you have not made all the requested setting in Internet Explorer per the Web Navigator manual. Normally, it takes about 10 minutes for WinCC users. The getting started section from the manual below is good to use. I normally test(web client install) on the same machine as the web server just to make sure everything is working before trying pc to pc. https://support.industry.siemens.com/cs/us/en/view/109746337 |
Follow us on