11/5/2012 5:49 PM | |
Posts: 60 Rating: (2) |
No this function? any one has solution? |
11/5/2012 7:21 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928) |
Havent tried this but you can try and let me know: In the alarm logging, you can create a message type.. In the message type properties you can set the text color as well as the background color for an alarm coming in, acknowledged and going out. If you set the acknowledgement theory (message class properties) to "Acknowledgement came in" then you can select "Flashing on" also. Please check if the alarmmessage is flashing the color you set in background... |
If I could help you, you can use the RATE button. Thank you. |
|
7/1/2013 10:44 AM | |
Posts: 60 Rating: (2) |
HiOreca, That what I said it only flashing the Text color, but not the Background colour. |
7/1/2013 11:26 AM | |
Joined: 4/17/2012 Last visit: 3/30/2024 Posts: 474 Rating: (10) |
Hi, find the attched file. for your reference
|
7/1/2013 11:42 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Battery Again??? |
VANDE MATARAM..... |
|
7/1/2013 11:48 AM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
dear DS, question is about flashing background from a message in the AlarmControl. Your example is about an object. These are 2 different things. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
Follow us on