7/11/2013 12:58 PM | |
Posts: 95 Rating: (10) |
hi is everybody that have any experience about connect wincc to Allen Bradly PLC? |
7/11/2013 1:03 PM | |
Posts: 1064 Rating: (72) |
wincc v7 has the drivers built in for allen bradley were as with wincc 6.2 use opc and rslinx .I have both running with out any issues |
7/11/2013 1:17 PM | |
Posts: 95 Rating: (10) |
hi playerslight can you give me more detail ? |
7/11/2013 1:21 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
All available with search function: WINCC COMMUNICATION Communication between Allen-Bradley ans WinCC7.1 and this the GOOGLE suggets: http://www.google.com/#sclient=psy-ab&q=allen+bradley%2Bcontrol+logix%2Bwincc%2Bopc&oq=allen+bradley%2Bcontrol+logix%2Bwincc%2Bopc&gs_l=hp.3...23081.23871.3.24076.4.4.0.0.0.0.752.752.6-1.1.0....0...1c.1.19.psy-ab.N3v5N6yofvw&pbx=1&bav=on.2,or.r_qf.&bvm=bv.48705608,d.aWc&fp=f63cc7b990c20fb7&biw=1252&bih=528 |
Last edited by: hdhosseini at: 7/11/2013 1:24 PM |
|
This contribution was helpful to2 thankful Users |
7/11/2013 1:29 PM | |
Posts: 1064 Rating: (72) |
What details do you require that's not covered by hdhosseini's reply |
7/11/2013 1:37 PM | |
Posts: 95 Rating: (10) |
can give me short explanation about connection via OPC? |
7/11/2013 1:43 PM | |
Joined: 1/20/2008 Last visit: 5/30/2024 Posts: 120 Rating: (7) |
Hello, I've done it twice with WinCC 7.0 SP3. Depending on the communication hardware used, the WinCC supports connections via the following channel units: Allen Bradley E/IP PLC5 Allen Bradley E/IP SLC50 Allen Bradley E/IP ControlLogix Please follow attached instruction. Regards, MRG AttachmentWinCC AB Help.pdf (186 Downloads) |
Last edited by: MRG at: 7/11/2013 2:49 PM |
|
7/11/2013 1:43 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, Have a look at this. What is OPC? - OPC DataHub |
VANDE MATARAM..... |
|
7/12/2013 9:37 AM | |
Posts: 95 Rating: (10) |
hi viralpatel you mean it dosent need external opc server? |