1/31/2011 11:56 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
I followed instructions found on this forum somewhere about changing "Structure Types" with the Configuration Tool. It might be possible that I did some changes while my project was in Runtime, so that might have caused some issues. script.exe & global script process are both running At the moment, I'm working with a backup from a few hours before these issues started cause I guess I would lose too much time trying to solve the damaged project. |
B r g d s , |
|
2/1/2011 1:11 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
I edited an existing Structure Type (adding extra elements) but it looked like changes in Excel were directly written to WinCC (without my confirmation). This, together with my fault that the project Runtime was activated at the same time, lead to this error. thanks for replying :) |
B r g d s , |
|
2/2/2011 9:29 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
Strange, after creating a new project, it also happens here. Seems like "script.exe" is killed at the same time, only message in log-files is:
|
B r g d s , |
|
2/2/2011 9:47 AM | |
Posts: 799 Rating: (43)
|
Hi SteBo, does there an Script.log file exists in diagnostic folder? regards |
2/2/2011 9:54 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
no, not in "C:\Program Files\Siemens\WinCC\diagnose" |
B r g d s , |
|
2/2/2011 10:04 AM | |
Posts: 799 Rating: (43)
|
that's not got!!! When script.exe really crashes and there is no logfile about it. Are you sure, that the process closes itself? If yes, you should install and configure the Microsoft Userdump tool for an automatic dump of the script.exe Download the tool here. Find detailed description here. If the error occurs again and a dumpfile is created you can be sure, that script.exe is crashing. For analysing the dumpfile you have to contac technical support. They will find out, what causes the crash. |
This contribution was helpful to1 thankful Users |
2/2/2011 10:27 AM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
thanks efka, I'll try that one Im' checking other log files: PMDiagnose.log:
|
B r g d s , |
|
2/2/2011 2:24 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
Followed User Mode Process Dumper as described but no dump... Still script.exe disappears. |
B r g d s , |
|
Follow us on