11/24/2022 3:01 AM | |
Joined: 9/4/2018 Last visit: 3/11/2024 Posts: 58 Rating: (0) |
Hi, I'm too facing this problem. My WinCC is 7.4 SP1. Due to problem with old PC, we changed it with new Dell PC in following steps. - OS : Windows 10 64 bit. Updated OS. - Installed WinCC. - Transferred Liecenses & Project backup too. It was working ok for 1 week. Later we got this message "WinCC Explorer - Server not Available" We downloaded the new OS Updates, but result was same. Later, I developed one temporary VB application & tried to connect dummy database in SQL Server. But it could not happend. Kindly guide how to resolve. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2022 09:17:57New subject after splitting |
|
11/24/2022 1:59 PM | |
Joined: 7/19/2022 Last visit: 4/26/2024 Posts: 356 Rating: (60) |
Hi GNit, This is most likely due to the fact that WinCC V7.4 SP1 is not compatible with your operating system. Please have a look at the attached Excel to check this. In case it is supported, it could be that the databases of a previous project are still connected to the WINCC SQL instance, cannot be reconnected and therefore the opening fails. Therefore, connect to SQL Server Management Studio to the WINCC SQL instance and check if the WinCC databases/segments are stuck. You may also find this FAQ useful, where the requirements for operating SIMATIC WinCC in a Windows network are discussed: What are the requirements for operating SIMATIC WinCC in a Windows network? AttachmentMicrosoft-Windows-10_en_2022-11-23.xlsx (184 Downloads) |
Last edited by: JBS98 at: 11/24/2022 14:01:58If this Information really helps, you could use the Rate function |
|
Follow us on