7/2/2012 8:14 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
First of all, there is not operating system Windows 7XP. Other thing, we need more info. Is it fresh install ? Maybe you have other version of SQL installed ? What other software do you have in your PC ? Also you can read this What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted? |
Best regards, |
|
7/2/2012 3:27 PM | |
Posts: 621 Rating: (10) |
Oh! sorry for wrong typed "Widows 7Xp" ie windows7. thank you very much for the reply i chek it & update the feedback |
7/8/2012 8:34 AM | |
Posts: 621 Rating: (10) |
Hi darius what you suggest above the link was i followed and also i formatted now windows XP sp2. now also iam facing the same problem also see the attached file Attachmenterror.zip (123 Downloads) |
7/10/2012 4:49 PM | |
Posts: 3037 Rating: (192)
|
Hello, you should do the point 1.4 in the following FAQ. What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted? Tweety |
7/12/2012 11:45 AM | |
Posts: 621 Rating: (10) |
Hi Tweety thanks for the reply as you suggested point 1.4 in the FAQ. this link same was darius also suggested. i was sollwed the same step by step even also not solved......! |
7/12/2012 12:50 PM | |
Posts: 3037 Rating: (192)
|
Hello, Do you use the right operating system? Do you use the rigth WinCC flexible version? You should check the list on the end of the following FAQ. With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible? Which version of WinCC flexible do you use? Do you install from CD? Tweety |
7/14/2012 11:21 AM | |
Posts: 621 Rating: (10) |
Hi darius / Tweety thank you for reply for this topic and keep in touch. finally i got the result. i was install the first seperatly MSQL 2005.and next i was install the software wincc flex2008. now working fine but inthere iam trying to install winccflex 2008 sp2.its asking please upgrade U13.what is that iand where can i down load that software..? |
7/16/2012 12:36 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello algudkar, Perhaps it means Update 13 for WinCC flexible 2008 SP2. You can download here: Update for WinCC flexible 2008 Service Pack 2 Best regards, Wizard |
8/29/2012 11:31 PM | |
Joined: 10/24/2011 Last visit: 2/23/2024 Posts: 4 Rating: (0) |
Hi algudkar, I am stuck in the same step you were at and cannot solve it. How did you make it? I am installing MS SQL 2005 first and got the error? After uninstall SQL, try to reinstall it, but always fail. Any suggestion are really appreciated. Best Regards, Jerry AttachmentC:\Documents and Settings\cma6499\My Documents\My Pictures\WinCC install error.JPG (100 Downloads) |
Follow us on