Industry Online Support
Technical Forum
2/22/2011 2:32 PM | |
Posts: 12 Rating: (0) |
Hello all. I am a little bit scary with all the things I read here. I have 20 valves, motors etc.. on a single view. I would like to display informations each time I click on them. I created faceplates, animated everything and really happy with this project! The only problem is that I cannot hide/show faceplates easily, that'sreally crazy! I followed this Siemens Tutorial:https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=23426416&nodeid0=16502367&caller=view&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW But I have to face something: some objects in the faceplate have already their visibility used by an other variable. How do you work when you have 20 motors on a single view?
Splitted from WinCC flexible: Visibility of a faceplate. |
Last edited by: O_Moderator at: 2/24/2011 9:49 AMnew subject after splitting |
|
2/24/2011 9:54 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread I made faceplates that are working pretty well and ready to use, but cannot change their visibility. Best regards O_Moderator |
Follow us on