6/16/2010 2:07 PM | |
Joined: 9/28/2005 Last visit: 7/10/2024 Posts: 2957 Rating: (242)
|
You can't upgrade Compact to Standard or Standard to Advanced. If you have Compact then you can upgrade it only to higher version, but it still be Compact. If you want to have Standard the you should buy Standard, but not upgrade. Its not possible. |
Best regards, |
|
6/16/2010 2:17 PM | |
Posts: 163 Rating: (0) |
for this requirement of ours,the local Siemens support has ordered 6AV6613-1XA51-3CE0...how is it going to solve the issue.... we need upgradation from 1)2005 to 2008 2)compact to Standard |
Last edited by: Sindhu at: 6/16/2010 2:18 PM |
|
6/16/2010 3:17 PM | |
Joined: 9/28/2005 Last visit: 7/10/2024 Posts: 2957 Rating: (242)
|
This is upgrade for runtime license from 2005 to 2008 version. Runtime licenses have no category such as Compact/Standard/Advanced. It is only for developement. So Siemens support suggested you to upgrade only RT license.
1. See my post above 2. Not possible. You should order Standard version separately with code 6AV6612-0AA51-3CA5 Please keep in mind that it is only possible to upgrade version, but not package type. You can't upgrade from Compact to Standard. You can upgrade the only version you have, I mean if you have Standard than you can upgrade it to newer Standard version. The same goes with Compact or Micro or Standard. |
Best regards, |
|
6/17/2010 8:25 AM | |
Posts: 163 Rating: (0) |
we have KTP1000 10.4" basic panel for which we need standard as per the attached picture found in one of the Siemens manuals. But we are convinced by local siemens support that Compact is Sufficient... Please discuss Attachmentcompact.zip (83 Downloads) |
6/17/2010 8:45 AM | |
Joined: 9/28/2005 Last visit: 7/10/2024 Posts: 2957 Rating: (242)
|
Comapct is enough. Look here http://support.automation.siemens.com/WW/view/en/28426206 |
Best regards, |
|
6/21/2010 2:50 PM | |
Joined: 4/24/2006 Last visit: 8/7/2024 Posts: 8711 Rating: (1166)
|
Dear Sindhu, When you have WinCC flexible Compact 2005, you can upgrade to WinCC flexible Compact 2008 ordering: 6AV6 611-0AA51-3CE5 Then you can order a Powerpack WinCC flexible Compact 2008 to WinCC flexible Standard 2008: 6AV6 612-2BC01-3AD5 Best regards, Wizard |
This contribution was helpful to1 thankful Users |
Follow us on